Glass Machinist Apprentice
Apply now »Date: Jul 3, 2022
Location: Canton, NY, US, 13617
Company: Corning
Requisition Number: 54516
Corning is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives.
Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges.
The purpose of this position is to plan, setup, program, precision machine, lightweight and measure high value hardware components, primarily for optical applications (mirrors). Operations include grinding, milling, lightweighting, contouring, vent holing, and other precision machining to meet customer specifications.
Job responsibilities include but are not limited to:
- Interpret customer and Corning internal drawings/blueprints of glass (mirror or other) parts and determine the approach to be used to meet specifications on 5-axis CNC machines, 5-axis AWJ machines, Large Campbell grinders, Northwoods vent hole machines or similar equipment used in the manufacturing of both solid and lightweight mirror components or other high precision parts requiring this type of equipment/process.
- Determine proper method and sequence to assemble and align workpiece support systems to tolerances of +/- 0.005”.
- Align workpieces within workspace to +/- 0.0005” tolerances.
- Prepare workpieces for machining operation, including the application of surface masks and loading on support bodies when required for part protection.
- Determine process details of how the parts will be loaded, held in place during machining, and unloaded from machine.
- Insert and secure residual handling devices.
- Manually remove residuals weighing in excess of 30 lbs. during AWJ lightweighting process.
- Operate material handling equipment such as overhead cranes, fork trucks, vacuum systems, and other material handling equipment to move heavy items up to 8 ton without damage.
- Determine what the optimum tooling, grits, speeds, feeds, lead angles are for machining, lightweighting or contouring of parts to insure features and dimensions specified are met.
- Able to hit tolerances as low as +/-0.001”.
- Manage machine/process operations through the CNC controller and process control computer.
- Initiate scripted machine actions via keyed inputs to CNC controller.
- Initiate manual motion of machine via keypad inputs and pushbuttons on controller.
- Interpret and react to system alarms.
- Monitor, measure, and generate process performance metrics through the use of handheld measurement tools and system-generated data.
- Maintain the high-pressure components of the system of the AWJ system.
- Perform removal, teardown, inspection, rebuild, installation and precision alignment of the nozzle assembly.
- Work in concert with trades personnel to replace high pressure hosing, piping, and rebuilding of intensifiers to ensure components meet specification and safety requirements.
- Perform scheduled lubrication and inspections of the manipulator.
- Calibrate and validate subsystem performance, including the abrasive valve and UHP (Ultra High-Pressure) pumps and nozzle performance.
- Work in a team environment with engineering, technical, production and project management personnel.
- Participate in the writing, revision and monitoring of Operating Procedures.
Graduate from SUNY Canton or similar education in Mechanical/Manufacturing Engineering Technology 2 year program in Glass Machinist classification or external machinist and CNC experience that is equivalent to this level of training.
We prohibit discrimination on the basis of race, color, gender, age, religion, national origin, sexual orientation, gender identity or expression, disability, veteran status or any other legally protected status.
We will ensure that individuals with disabilities are provided reasonable accommodation to participate in the job application or interview process, to perform essential job functions, and to receive other benefits and privileges of employment. Please contact us to request accommodation.
Nearest Major Market: Massena